FXOS8700 linux driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FXOS8700 linux driver

2,042 次查看
maximkuk
Contributor III

Hello!

In our custom board we use FXOS8700. When I start driver from fsl-arm-yocto-bsp (kernel 4.9.11), I see that it creates only one input device and event from accelerometer and magnetometer are emitting from one source, so I can't use acc and mag devices simultaneously.

I modifyed fxos8700 driver to create two input devices - separately for acc and mag. I think it will be useful to share this patch :smileyhappy:.

标签 (5)
标记 (3)
0 项奖励
回复
2 回复数

1,667 次查看
pandaerliu
Contributor II

The patch fixed my problem.Thank you very much for sharing.

0 项奖励
回复

1,667 次查看
maximkuk
Contributor III

Or there is another version of this driver from here: https://community.nxp.com/thread/330614 

0 项奖励
回复