FXOS8700 linux driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXOS8700 linux driver

2,744件の閲覧回数
maximkuk
Contributor III

Hello!

In our custom board we use FXOS8700. When I start driver from fsl-arm-yocto-bsp (kernel 4.9.11), I see that it creates only one input device and event from accelerometer and magnetometer are emitting from one source, so I can't use acc and mag devices simultaneously.

I modifyed fxos8700 driver to create two input devices - separately for acc and mag. I think it will be useful to share this patch :smileyhappy:.

ラベル(5)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,369件の閲覧回数
pandaerliu
Contributor II

The patch fixed my problem.Thank you very much for sharing.

0 件の賞賛
返信

2,369件の閲覧回数
maximkuk
Contributor III

Or there is another version of this driver from here: https://community.nxp.com/thread/330614 

0 件の賞賛
返信