Ethernet speed problem on i.MX6 platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet speed problem on i.MX6 platform

ソリューションへジャンプ
2,844件の閲覧回数
DeweyM_D_Jang
Contributor I

I've tested Ethernet speed on i.MX6 Sabre-SD board and found a strange problem.

When I download a file using ftpget command from a FTP server on Ubuntu PC(vsftpd), the transfer speed is good(over 30Mbps).

But from a FTP server on Windows PC(Cerberus FTP server) within the same network, the transfer speed is very poor(about 3Mbps).

LTIB version 12.09 S/W platform and 100baseTx-FD network.

I wonder what caused this difference.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,513件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

As you mentioned there is no problem on Ubuntu PC(vsftpd) but slow transfer speed on Windows PC(Cerberus FTP server). That means the  i.MX6 Sabre-SD board is work well. The problem may due to the setting different in Cerberus FTP server. Is there any speed limitation setting in Cerberus FTP server?

Someone also met the slow transfer speed:

http://www.cerberusftp.com/search.html?cx=007223768916750377522%3Auo72hiszuwa&cof=FORID%3A10%3BNB%3A...

Hope this information can help you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,514件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

As you mentioned there is no problem on Ubuntu PC(vsftpd) but slow transfer speed on Windows PC(Cerberus FTP server). That means the  i.MX6 Sabre-SD board is work well. The problem may due to the setting different in Cerberus FTP server. Is there any speed limitation setting in Cerberus FTP server?

Someone also met the slow transfer speed:

http://www.cerberusftp.com/search.html?cx=007223768916750377522%3Auo72hiszuwa&cof=FORID%3A10%3BNB%3A...

Hope this information can help you.

0 件の賞賛
返信