Ethernet speed problem on i.MX6 platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet speed problem on i.MX6 platform

Jump to solution
2,750 Views
DeweyM_D_Jang
Contributor I

I've tested Ethernet speed on i.MX6 Sabre-SD board and found a strange problem.

When I download a file using ftpget command from a FTP server on Ubuntu PC(vsftpd), the transfer speed is good(over 30Mbps).

But from a FTP server on Windows PC(Cerberus FTP server) within the same network, the transfer speed is very poor(about 3Mbps).

LTIB version 12.09 S/W platform and 100baseTx-FD network.

I wonder what caused this difference.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,419 Views
jimmychan
NXP TechSupport
NXP TechSupport

As you mentioned there is no problem on Ubuntu PC(vsftpd) but slow transfer speed on Windows PC(Cerberus FTP server). That means the  i.MX6 Sabre-SD board is work well. The problem may due to the setting different in Cerberus FTP server. Is there any speed limitation setting in Cerberus FTP server?

Someone also met the slow transfer speed:

http://www.cerberusftp.com/search.html?cx=007223768916750377522%3Auo72hiszuwa&cof=FORID%3A10%3BNB%3A...

Hope this information can help you.

View solution in original post

0 Kudos
Reply
1 Reply
1,420 Views
jimmychan
NXP TechSupport
NXP TechSupport

As you mentioned there is no problem on Ubuntu PC(vsftpd) but slow transfer speed on Windows PC(Cerberus FTP server). That means the  i.MX6 Sabre-SD board is work well. The problem may due to the setting different in Cerberus FTP server. Is there any speed limitation setting in Cerberus FTP server?

Someone also met the slow transfer speed:

http://www.cerberusftp.com/search.html?cx=007223768916750377522%3Auo72hiszuwa&cof=FORID%3A10%3BNB%3A...

Hope this information can help you.

0 Kudos
Reply