Ethernet speed problem on i.MX6 platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ethernet speed problem on i.MX6 platform

跳至解决方案
2,757 次查看
DeweyM_D_Jang
Contributor I

I've tested Ethernet speed on i.MX6 Sabre-SD board and found a strange problem.

When I download a file using ftpget command from a FTP server on Ubuntu PC(vsftpd), the transfer speed is good(over 30Mbps).

But from a FTP server on Windows PC(Cerberus FTP server) within the same network, the transfer speed is very poor(about 3Mbps).

LTIB version 12.09 S/W platform and 100baseTx-FD network.

I wonder what caused this difference.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,426 次查看
jimmychan
NXP TechSupport
NXP TechSupport

As you mentioned there is no problem on Ubuntu PC(vsftpd) but slow transfer speed on Windows PC(Cerberus FTP server). That means the  i.MX6 Sabre-SD board is work well. The problem may due to the setting different in Cerberus FTP server. Is there any speed limitation setting in Cerberus FTP server?

Someone also met the slow transfer speed:

http://www.cerberusftp.com/search.html?cx=007223768916750377522%3Auo72hiszuwa&cof=FORID%3A10%3BNB%3A...

Hope this information can help you.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,427 次查看
jimmychan
NXP TechSupport
NXP TechSupport

As you mentioned there is no problem on Ubuntu PC(vsftpd) but slow transfer speed on Windows PC(Cerberus FTP server). That means the  i.MX6 Sabre-SD board is work well. The problem may due to the setting different in Cerberus FTP server. Is there any speed limitation setting in Cerberus FTP server?

Someone also met the slow transfer speed:

http://www.cerberusftp.com/search.html?cx=007223768916750377522%3Auo72hiszuwa&cof=FORID%3A10%3BNB%3A...

Hope this information can help you.

0 项奖励
回复