Enable kernel configuration options like CONFIG_PROFILING and CONFIG_PERF_EVENTS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable kernel configuration options like CONFIG_PROFILING and CONFIG_PERF_EVENTS

2,301 Views
mohamad-ahmad
Contributor III

Hello,

Can someone help me how I can change the kernel configurations by enabling certain of them like CONFIG_PERF_EVENTS and CONFIG_PROFILING.

Normally when I check some configurations I find, for example:

# XXXXXX is not set

or

YYYYYY=y

Thank you for the help

Labels (1)
0 Kudos
Reply
2 Replies

1,729 Views
mohamad-ahmad
Contributor III

thank you Yuri.

Mohamad

0 Kudos
Reply

1,728 Views
Yuri
NXP Employee
NXP Employee

Hello,

The following may be useful :

Task #5 - Kernel

i.MX Yocto Project: How can I patch the kernel?

i.MX Yocto Project: How can I compile the kernel manually?

i.MX Yocto Project: Frequently Asked Questions

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply