Enable Phonegap framework and java for IMX6q using LTIB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable Phonegap framework and java for IMX6q using LTIB

1,595 Views
shalinikp
Contributor II

Is it possible to enable phonegap and java on LTIB for imx6q.  Please reply if any one has enabled it.

Labels (2)
0 Kudos
Reply
1 Reply

1,476 Views
b36401
NXP Employee
NXP Employee

Java virtual machines are able to run on the MX6x BSPs. However we do not offer any java VM in the BSP.

Oracle has pre-built versions of Java Virtual Machine for ARM Processors. It's possible to download them here:

http://www.oracle.com/technetwork/java/embedded/embedded-se/downloads/index.html

You can find mode details in this document:

https://community.freescale.com/docs/DOC-1478

0 Kudos
Reply