About adjustment function of SDHC in i.MX6SDL.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About adjustment function of SDHC in i.MX6SDL.

1,159 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

I have a question about adjustment function of SDHC in i.MX6SDL.

I got the information that i.MX6 has Variable_Output_Data_Window(CMD19) function from below URL.

https://community.freescale.com/thread/334945

[Question]

[Q1]

When the adjustment specification of the SD card is tOP = 0~2[UI], is it possible to adjust regardless of the relation with the propagation-delay-time of the clock and data?

[Q2]

How is a sample point of host side fixed (adjusted) in Variable-clock function?

There is below description in SD Phsical Layer Specification V4.20.

"At the initialization step the host should take care to find the optimal sampling point for the card outputs."

Is this adjusted for the setup and hold to become a center?

(If it's yes, how much does the looseness occur?)

Best Regards,

Keita

标签 (5)
0 项奖励
回复
2 回复数

1,045 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

please elevate this through local FAE

(reason is that I have big difficulties to understand questions).

Thanks.

Best regards

igor

0 项奖励
回复

1,045 次查看
keitanagashima
Senior Contributor I

Dear Igor,

Hello.

Sorry for my poor question.

I will re-post this question to understand easily.

So, I'll remove this request.

BR,

Keita

0 项奖励
回复