Hi,
we own a i.MX28 EVK and I switched of the Board while Linux was running - now the ext2 filesystem is broken and the gui doesn't come up.
I would like to bring the SD card to the "factory default", as it was delivered with the evaluation kit. I already downloaded
but now I'm stuck and don't know how to use the tool and the files. I tried
CFImager.exe -d f -f rootfs.ext2
and
CFImager.exe -d f -f imx28_uboot.sb
but in both cases when I insert the card into the i.MX28 EVK the serial console just outputs a hexadecimal number instead of booting, e.g.
0x80502008
How can I write the Linux Image that was shipped with the board to a SD card?
Thanks
Christoph
Hi
If you have linux, then follow the steps in this blog
http://importgeek.wordpress.com/2014/07/25/burning-imx28-ltib-image-to-sd-card-and-booting/
Regards
Pt
Thanks, but unfortunately ;-) we're using windows.
I do have the option to grab a computer and install linux, but hopefully there's an easier way to write the sd card image under windows ...
Thanks for the error codes.
I tried flashing the sd card with the -a option, as suggested:
C:\Temp\CFImager.v1.7.3.001_bin+src>CFImager.exe -f imx28_uboot.sb -d f -a
drive = F
removable = no
device block size = 512 bytes
device block count = 0xeccc46
firmware size = 0x224b0 bytes (0x113 blocks)
extra blocks = 1772
Writing LDT...
Writing firmware...
Writing FAT partition...
Writing MBR...
done!
C:\Temp\CFImager.v1.7.3.001_bin+src>
The error codes I'm getting are as follows:
*plug in power*
0x8050100f
0x8050100f
*some time elapses*
0x80502008
0x8050100f
*some time elapses*
0x80502008
0x8050100f
*some time elapses*
...
Am I flashing the correct file (imx28_uboot.sb)?
I probably need to copy the file system onto the SD card, too - how would I do that?
Thanks
Christoph
Hi
Try to use imx28_ivt_uboot.sb (The i.MX28 EVK is HAB enabled by default)
Booting and Testing IMX287 evk
Regards
Pt