EIM: Muxed 16-bit NOR Flash Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

EIM: Muxed 16-bit NOR Flash Example

跳至解决方案
2,512 次查看
norishinozaki
Contributor V

Hello Champs,

A customer is asking for schematics or diagrams which use a 16-bit multiplexed NOR Flash connected to EIM.

I found some of SPI NOR Flash cases but none of EIM.

Please introduce if there is any.

Best regards,

Nori Shinozaki

标签 (1)
0 项奖励
回复
1 解答
2,390 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,391 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
2,392 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nori

I think below diagram may be useful

Muxed Mode.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复