EIM: Muxed 16-bit NOR Flash Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EIM: Muxed 16-bit NOR Flash Example

ソリューションへジャンプ
2,515件の閲覧回数
norishinozaki
Contributor V

Hello Champs,

A customer is asking for schematics or diagrams which use a 16-bit multiplexed NOR Flash connected to EIM.

I found some of SPI NOR Flash cases but none of EIM.

Please introduce if there is any.

Best regards,

Nori Shinozaki

ラベル(1)
0 件の賞賛
返信
1 解決策
2,393件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,394件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,395件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

I think below diagram may be useful

Muxed Mode.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信