EIM: Muxed 16-bit NOR Flash Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EIM: Muxed 16-bit NOR Flash Example

Jump to solution
2,510 Views
norishinozaki
Contributor V

Hello Champs,

A customer is asking for schematics or diagrams which use a 16-bit multiplexed NOR Flash connected to EIM.

I found some of SPI NOR Flash cases but none of EIM.

Please introduce if there is any.

Best regards,

Nori Shinozaki

Labels (1)
0 Kudos
Reply
1 Solution
2,388 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
2,389 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,390 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

I think below diagram may be useful

Muxed Mode.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply