HDMI Interlaced Mode Timing Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HDMI Interlaced Mode Timing Issue

ソリューションへジャンプ
2,214件の閲覧回数
jonchaps
Contributor II

Hello,


The patches published at Patch for iMX6 BSP to support interlaced display on HDMI and LCD interface, which added support for HDMI interlaced modes on the iMX6, do not adhere to the timing requirements specified in the CEA-861 specification.


After applying the new version of "patch4" from the thread specified above, there is a timing issue where the VSYNC signal is offset by one pixel clock from where it should be. The CEA-861 specification states that the VSYNC should be perfectly aligned with the HSYNC signal plus or minus zero pixel clocks for field 1. For field 2 the VSYNC should be Htotal/2 pixel clocks from the leading edge of the HSYNC signal plus or minus zero pixel clocks. In both cases the VSYNC is 1 pixel clock too late. Is there a way to correct this offset on the IPU so that this functions according to the CEA spec?


I raised this issue in the original thread (HDMI Interlaced Modes), but that thread no longer appears to be active.


Thank you,

Jon

ラベル(1)
0 件の賞賛
返信
1 解決策
1,862件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,863件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信