Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

926 次查看
m_c
Senior Contributor I

Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

标签 (2)
0 项奖励
回复
1 回复

728 次查看
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

IPU CSI supported resolutions do not depend on sync mode and

CSI BT.656 can be supported with these resolutions too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复