Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

960件の閲覧回数
m_c
Senior Contributor I

Does i.MX6 Solo CSI BT.656 embedded sync mode can support resolution higher than D1 (Ex: 720p, 1080p)?

ラベル(2)
0 件の賞賛
返信
1 返信

762件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

IPU CSI supported resolutions do not depend on sync mode and

CSI BT.656 can be supported with these resolutions too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信