Loading custom Image to eMMC using Mfgtools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Loading custom Image to eMMC using Mfgtools

2,446 Views
guna007
Contributor III

We have a custom board based on imx6q and we have built our image using yocto project. How can I load my custom image to eMMC in my board using Mfgtools provided by NXP/Freescale?

Note:I have built initramfs using "bitbake fsl-image-mfgtool-initramfs" command.

Labels (3)
0 Kudos
Reply
1 Reply

1,839 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gunasekaran

old mfg tool files should be replaced with new in folder

Profile/Linux/OS Firmware/firmware/

Image files are in folder ../files

Just for reference one can look at attached Linux Guide p.15.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply