6UL Simplified power design ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

6UL Simplified power design ?

1,233 次查看
SJA
Contributor II

We have a design with no need for any power saving modes.

Can we use a simplified power design with two rails 3.3v and 1.35v ?

1.35v would feed VDD_SOC_IN and NVCC_DRAM (and DRAM VCC)

3.3v would feed VDD_HIGH_IN, VDD_SNVS_IN and the other NVCC peripheral rails.

0 项奖励
回复
1 回复

1,144 次查看
igorpadykov
NXP Employee
NXP Employee

Hi SJA

yes seems this is possible, also power-up sequence should be

observed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复