DDR3 routing, length matching

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 routing, length matching

ソリューションへジャンプ
2,522件の閲覧回数
celiley
Contributor I

Hello,

There is a point I'm not sure about DDR3 routing. I'm following "Hardware Development Guide for
i.MX 6Quad" and this document says that the address signals must match 25 mils. When calculating the length of each signal, must we add the vias' length in the z direction to the total length? In my design, each address signal has the same number of vias but I drew some of the signals on different intermediate layers. When I add the depth of the via to the total length, there is a difference of about 150 mils. What do you suggest about it, what is the correct calculation in DDR3 routing?

Thanks, regards,

Celile

ラベル(1)
0 件の賞賛
返信
1 解決策
2,472件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Celile

 

yes vias length must be added to calculation. In general also may be recommended to perform

ibis modelling.

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,473件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Celile

 

yes vias length must be added to calculation. In general also may be recommended to perform

ibis modelling.

 

Best regards
igor

0 件の賞賛
返信
2,462件の閲覧回数
celiley
Contributor I

Thank you @igorpadykov 

0 件の賞賛
返信