DDR3 routing, length matching

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR3 routing, length matching

跳至解决方案
1,598 次查看
celiley
Contributor I

Hello,

There is a point I'm not sure about DDR3 routing. I'm following "Hardware Development Guide for
i.MX 6Quad" and this document says that the address signals must match 25 mils. When calculating the length of each signal, must we add the vias' length in the z direction to the total length? In my design, each address signal has the same number of vias but I drew some of the signals on different intermediate layers. When I add the depth of the via to the total length, there is a difference of about 150 mils. What do you suggest about it, what is the correct calculation in DDR3 routing?

Thanks, regards,

Celile

标签 (1)
0 项奖励
回复
1 解答
1,548 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Celile

 

yes vias length must be added to calculation. In general also may be recommended to perform

ibis modelling.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,549 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Celile

 

yes vias length must be added to calculation. In general also may be recommended to perform

ibis modelling.

 

Best regards
igor

0 项奖励
回复
1,538 次查看
celiley
Contributor I

Thank you @igorpadykov 

0 项奖励
回复