DDR Stress Tester

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,717件の閲覧回数
shojigoto
Contributor II

Is the DDR Stress Tester able to be available on the i.MX6Q without any boot program installed?

We are now facing a problem of DDR reset from i.MX6 being never deassetred after power-on, and

so the DDR stress Tester fails in executing DDR Calibration.

Regards,

Shoji

ラベル(1)
0 件の賞賛
返信
1 解決策
2,511件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shoji

from i.MX6DQ Datasheet (rev.4, 7/2015) Table 6. Operating Ranges :

This supply also powers the pre-drivers of the DDR I/O pins; therefore,

it must always be provided, even when LVDS is not used.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

~igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,511件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shoji

one can use jtag version

i.MX6/7 DDR Stress Test Tool V2.20

also pin DRAM_RESET after power-up is low according to Table 100. 21 x 21

mm Functional Contact Assignments (continued) i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,511件の閲覧回数
shojigoto
Contributor II

Hi igor,

Thank you for your reply.

I found that a power line NVCC_LVDS_2P5 is left open on our board.

Could you tell me whether accessing to the DDR3 is possible in that case?

Regards,

Shoji

0 件の賞賛
返信
2,512件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shoji

from i.MX6DQ Datasheet (rev.4, 7/2015) Table 6. Operating Ranges :

This supply also powers the pre-drivers of the DDR I/O pins; therefore,

it must always be provided, even when LVDS is not used.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

~igor

0 件の賞賛
返信