why the ipu csi can handled up to 4 streams of data in imx6d.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why the ipu csi can handled up to 4 streams of data in imx6d.

724件の閲覧回数
guanliangding
Contributor III

Hi, all:

     In imx6d, ipu csi is selected to get one of vc. This is a compatible design?

0 件の賞賛
返信
1 返信

642件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi guanliang

vc selection can be understood from i.MX6DQ RM  Chapter 19

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信