DDR Stress Tester

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Tester

Jump to solution
2,761 Views
shojigoto
Contributor II

Is the DDR Stress Tester able to be available on the i.MX6Q without any boot program installed?

We are now facing a problem of DDR reset from i.MX6 being never deassetred after power-on, and

so the DDR stress Tester fails in executing DDR Calibration.

Regards,

Shoji

Labels (1)
0 Kudos
Reply
1 Solution
2,555 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shoji

from i.MX6DQ Datasheet (rev.4, 7/2015) Table 6. Operating Ranges :

This supply also powers the pre-drivers of the DDR I/O pins; therefore,

it must always be provided, even when LVDS is not used.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

~igor

View solution in original post

0 Kudos
Reply
3 Replies
2,555 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shoji

one can use jtag version

i.MX6/7 DDR Stress Test Tool V2.20

also pin DRAM_RESET after power-up is low according to Table 100. 21 x 21

mm Functional Contact Assignments (continued) i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,555 Views
shojigoto
Contributor II

Hi igor,

Thank you for your reply.

I found that a power line NVCC_LVDS_2P5 is left open on our board.

Could you tell me whether accessing to the DDR3 is possible in that case?

Regards,

Shoji

0 Kudos
Reply
2,556 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shoji

from i.MX6DQ Datasheet (rev.4, 7/2015) Table 6. Operating Ranges :

This supply also powers the pre-drivers of the DDR I/O pins; therefore,

it must always be provided, even when LVDS is not used.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

~igor

0 Kudos
Reply