Can I use external oscillator with spread spectrum function?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I use external oscillator with spread spectrum function?

跳至解决方案
1,329 次查看
tomo
Contributor II

Hello,

Can I use 24MHz external oscillator with spread spectrum function to the i.MX6 processor?

Or, is there another way to use?

Best Regards,

Tomo

标签 (1)
0 项奖励
回复
1 解答
1,224 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tomokazu

in general this is not recommended due to restrictions in

sect.2.7 Oscillator tolerance IMX6DQ6SDLHDG

System PLL supports spread spectrum modulation

described in sect.18.5.1.3.3 System PLL IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,225 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tomokazu

in general this is not recommended due to restrictions in

sect.2.7 Oscillator tolerance IMX6DQ6SDLHDG

System PLL supports spread spectrum modulation

described in sect.18.5.1.3.3 System PLL IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复