Can I use external oscillator with spread spectrum function?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use external oscillator with spread spectrum function?

ソリューションへジャンプ
1,337件の閲覧回数
tomo
Contributor II

Hello,

Can I use 24MHz external oscillator with spread spectrum function to the i.MX6 processor?

Or, is there another way to use?

Best Regards,

Tomo

ラベル(1)
0 件の賞賛
返信
1 解決策
1,232件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tomokazu

in general this is not recommended due to restrictions in

sect.2.7 Oscillator tolerance IMX6DQ6SDLHDG

System PLL supports spread spectrum modulation

described in sect.18.5.1.3.3 System PLL IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,233件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tomokazu

in general this is not recommended due to restrictions in

sect.2.7 Oscillator tolerance IMX6DQ6SDLHDG

System PLL supports spread spectrum modulation

described in sect.18.5.1.3.3 System PLL IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信