i.MX6 - UART DTE-DCE mode -> Figure 64.2 in Reference Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 - UART DTE-DCE mode -> Figure 64.2 in Reference Manual

ソリューションへジャンプ
3,062件の閲覧回数
g_moreno
Contributor III

Hello,

I'm wondering if there is a mistake or if I am misunderstanding what figure 64.2 in the i.MX6DQ RM states.

According to:

64.4.3.3 DTR_B: Input in DCE mode and output in DTE mode.

64.4.3.4 DSR_B: Output in DCE mode and input in DTE mode.

64.4.3.6 DCD_B: Output in DCE mode and input in DTE mode

64.4.3.7 RI_B: Output in DCE mode and input in DTE mode.

Ignoring the IOMUX function, figure 64.2 shows the exact opposite directions for these 4 signals in both DTE and DCE modes.

TX_DATA, RX_DATA, CTS_B and RTS_B behave as inputs or outputs, independent from DTE or DCE configurations, but the modem signals just don't match in this figure.

Am I getting a wrong interpretation here?

Thanks,

Guillermo

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,646件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guillermo

your interpretation is correct. In general recommended to use

Table 90. UART I/O Configuration vs. Mode IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guillermo

your interpretation is correct. In general recommended to use

Table 90. UART I/O Configuration vs. Mode IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,646件の閲覧回数
g_moreno
Contributor III

Hello Igor,

Thanks for clarifying this.

Best regards,

Guillermo

0 件の賞賛
返信