Can I use external oscillator with spread spectrum function?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use external oscillator with spread spectrum function?

Jump to solution
1,202 Views
tomo
Contributor II

Hello,

Can I use 24MHz external oscillator with spread spectrum function to the i.MX6 processor?

Or, is there another way to use?

Best Regards,

Tomo

Labels (1)
0 Kudos
Reply
1 Solution
1,097 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tomokazu

in general this is not recommended due to restrictions in

sect.2.7 Oscillator tolerance IMX6DQ6SDLHDG

System PLL supports spread spectrum modulation

described in sect.18.5.1.3.3 System PLL IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,098 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tomokazu

in general this is not recommended due to restrictions in

sect.2.7 Oscillator tolerance IMX6DQ6SDLHDG

System PLL supports spread spectrum modulation

described in sect.18.5.1.3.3 System PLL IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply