Boot from QSPI-NOR flash without SDcard on IMX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot from QSPI-NOR flash without SDcard on IMX7

Jump to solution
1,390 Views
JAEWON
Contributor I

i'm using a i.MX7Dual SABRE and I want to boot use QSPI-NOR flash. 

but for my personal reasons, I can't use the SD card.

I changed the resistance setting by referring to the post below and tried to write without SD card using mfgtool, but it did not work as expected. Is this impossible at all or am I not trying to do it right?

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Write-program-to-the-QSPI-NOR-on-i-MX-7D...

Labels (1)
0 Kudos
Reply
1 Solution
1,380 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the MCIMX7SABRE  board from NXP? If yes,  you need to follow it.

 

View solution in original post

0 Kudos
Reply
3 Replies
1,381 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the MCIMX7SABRE  board from NXP? If yes,  you need to follow it.

 

0 Kudos
Reply
1,379 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using?

0 Kudos
Reply
1,357 Views
JAEWON
Contributor I

Sorry for my belated reply. 

I couldn't care because of the holidays and other tasks.The BSP version I'm currently using is 5.4.70_2.3.0, and it seems to be a problem with the board from what the company found out.
Because it is not a regular board, but a little customized board.

 

Thanks for your answer.

0 Kudos
Reply