IMX8M booting options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8M booting options

ソリューションへジャンプ
1,825件の閲覧回数
Luishernandez1
Contributor II

Hi everyone,

 

Want to confirm that the IMX8M Nano supports booting off the below linked NAND through the GPMI interface.

https://4donline.ihs.com/images/VipMasterIC/IC/FASL/FASLS03878/FASLS03878-1.pdf?hkey=52A5661711E4025...

 

Regards,

Israel H.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,818件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi Luishernandez1,

 

Reviewing the datasheet from the NAND and the iIMX8M nano it should be compatible with no further problems, also one can check the reference manual on the chapter 6.1.5 Boot devices (internal boot), please take a look on the fragment from the manual:

- Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2
interface, located at CS0. Page sizes of 2 KB, 4 KB, and 8 KB. The bus widths of 8-
bit with 2 through 62-bit BCH hardware ECC (Error Correction) are supported.

 

Regards,

Israel H.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,819件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi Luishernandez1,

 

Reviewing the datasheet from the NAND and the iIMX8M nano it should be compatible with no further problems, also one can check the reference manual on the chapter 6.1.5 Boot devices (internal boot), please take a look on the fragment from the manual:

- Raw NAND (MLC and SLC), and Toggle-mode NAND flash through GPMI-2
interface, located at CS0. Page sizes of 2 KB, 4 KB, and 8 KB. The bus widths of 8-
bit with 2 through 62-bit BCH hardware ECC (Error Correction) are supported.

 

Regards,

Israel H.

0 件の賞賛
返信