Boot from QSPI-NOR flash without SDcard on IMX7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot from QSPI-NOR flash without SDcard on IMX7

ソリューションへジャンプ
1,410件の閲覧回数
JAEWON
Contributor I

i'm using a i.MX7Dual SABRE and I want to boot use QSPI-NOR flash. 

but for my personal reasons, I can't use the SD card.

I changed the resistance setting by referring to the post below and tried to write without SD card using mfgtool, but it did not work as expected. Is this impossible at all or am I not trying to do it right?

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Write-program-to-the-QSPI-NOR-on-i-MX-7D...

ラベル(1)
0 件の賞賛
返信
1 解決策
1,400件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the MCIMX7SABRE  board from NXP? If yes,  you need to follow it.

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,401件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the MCIMX7SABRE  board from NXP? If yes,  you need to follow it.

 

0 件の賞賛
返信
1,399件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using?

0 件の賞賛
返信
1,377件の閲覧回数
JAEWON
Contributor I

Sorry for my belated reply. 

I couldn't care because of the holidays and other tasks.The BSP version I'm currently using is 5.4.70_2.3.0, and it seems to be a problem with the board from what the company found out.
Because it is not a regular board, but a little customized board.

 

Thanks for your answer.

0 件の賞賛
返信