Applying LPDDR2 on MX6DQ issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Applying LPDDR2 on MX6DQ issues

Jump to solution
2,837 Views
raymondwang
Senior Contributor I

Recently we are trying to apply LPDDR2 on MX6DQ. There are some questions we need to know. Please help us if you has same experience.

1. How about LPDDR2 single channel or dual channel?

    We use an eMCP packged LPDDR2 chip from Samsung with PN KMK7X000VM. It including two internal LPDDR2 chips (two cs,128Mbx32,totally 8Gb).

    How can set mx6 MMDC controller? For our design, can use config it with single channel or dual channel freely?

   Any patch is welcome!

2.Currently our kernel version is 3.0.25 (android 4.2.2 1.1.0 based on). I think it does have LPDDR2 support in kernel mx6_mmdc.c and suspend/resume handling

code.

  Any one has patch for linux kernel mx6q LPDDR2?

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,207 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raymond

you can use both single channel or dual channel, also

please look at links below

https://community.freescale.com/message/338104#338104

i.MX6DL LPDDR2 Support for L3.0.35_4.0.0

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,208 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raymond

you can use both single channel or dual channel, also

please look at links below

https://community.freescale.com/message/338104#338104

i.MX6DL LPDDR2 Support for L3.0.35_4.0.0

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,207 Views
raymondwang
Senior Contributor I

Great! Thanks!

0 Kudos
Reply