Applying LPDDR2 on MX6DQ issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Applying LPDDR2 on MX6DQ issues

ソリューションへジャンプ
2,795件の閲覧回数
raymondwang
Senior Contributor I

Recently we are trying to apply LPDDR2 on MX6DQ. There are some questions we need to know. Please help us if you has same experience.

1. How about LPDDR2 single channel or dual channel?

    We use an eMCP packged LPDDR2 chip from Samsung with PN KMK7X000VM. It including two internal LPDDR2 chips (two cs,128Mbx32,totally 8Gb).

    How can set mx6 MMDC controller? For our design, can use config it with single channel or dual channel freely?

   Any patch is welcome!

2.Currently our kernel version is 3.0.25 (android 4.2.2 1.1.0 based on). I think it does have LPDDR2 support in kernel mx6_mmdc.c and suspend/resume handling

code.

  Any one has patch for linux kernel mx6q LPDDR2?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
2,165件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raymond

you can use both single channel or dual channel, also

please look at links below

https://community.freescale.com/message/338104#338104

i.MX6DL LPDDR2 Support for L3.0.35_4.0.0

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,166件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raymond

you can use both single channel or dual channel, also

please look at links below

https://community.freescale.com/message/338104#338104

i.MX6DL LPDDR2 Support for L3.0.35_4.0.0

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,165件の閲覧回数
raymondwang
Senior Contributor I

Great! Thanks!

0 件の賞賛
返信