ADV7280-m clock issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADV7280-m clock issue

7,576 次查看
kurkinalexandr
Contributor III

Hello.

Currently I am working on driver integration task for adv7280-m chip.

And I got issue related to mipi csi clock. Mipi dphy driver detect Clock line as ULPS(ultralow power state).  You can see my oscilloscope images in this branch adv7280-M clock problem | EngineerZone .

I am trying to understand what could be the reason of issue: adv7280-m chip or imx6. Could anybody, who  worked with this adv7280-m chip show me your signals on the mipi lines or analize my signals.

I also interested in what should be switched on first: the decoder chip mipi dphy or  imx6 mipi dphy.

As I understand. there are a lot of people who managed to get workable adv7280-m chip with imx6. Could you also share your mipi csi2 driver settup

Thanks.

标记 (3)
12 回复数

6,534 次查看
igorpadykov
NXP Employee
NXP Employee

I have not adv7280 but one can attach external termination resistors and check.

0 项奖励
回复

6,534 次查看
kurkinalexandr
Contributor III

Unfortunately it is difficult to solder this termination resistor on our board. May be we will order ADV7280-m kit and connect it to CM-FX6 kit or Sabre board.

Could you explane me some points related to MIPI_CSI_PHY_STATE.

First of all 9-th bit. Active low. Is that mean that clk lane in ULPS if the bit equel zero value?

8-th bit. Clock lane actively receiving a DDR cloclk. Is that bit mean(1-value) that imx6 DPHY module clock is correctly configured. In my case it is always zero value.

Thanks.

0 项奖励
回复

6,534 次查看
igorpadykov
NXP Employee
NXP Employee

please create new thread for new questions

Best regards

igor

0 项奖励
回复

6,534 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fan

I would suggest to configure properly i.MX6 mipi clock as described in

Debug steps for customer MIPI sensor.docx

A Simple tutor for writing i.MX6 mipi driver, use adv7480 as an example

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

6,534 次查看
kurkinalexandr
Contributor III

Hi Igor.

Do you think it is correct that transition from 1.2V to 0.1-0,2V on CLK line was detected as ULPS by imx6(0x210 in state register)?

Thanks.

0 项奖励
回复

6,534 次查看
igorpadykov
NXP Employee
NXP Employee

I think yes it can be detected in MIPI_CSI_PHY_STATE register bit 9.

Best regards

igor

0 项奖励
回复

6,534 次查看
kurkinalexandr
Contributor III

But ULPS mode should have 0V level on lines. In our case we have 0,1-0,2V and it is high speed level according to DPHY specification.

0 项奖励
回复

6,534 次查看
igorpadykov
NXP Employee
NXP Employee

are you sure that this is not noise, as is ULPS mode

sensor can turn off supplies from lane.

Also this can be quality issue, so recommended to double

check behaviour on other board/sensor.

0 项奖励
回复

6,534 次查看
kurkinalexandr
Contributor III

As I understand, imx6 should detect 1.2 >0.1V transition(low power -> high speed) and set termination on the line. If  it detect this transition as ULPS, it of course will not set termination and future signal on the line will be not correct(noise in my case as you said).

Do you have any opportunity to get signal oscilloscope  images in case of correct imx6-adv7280-m work?

0 项奖励
回复

6,534 次查看
kurkinalexandr
Contributor III

Hello.

Thank you for replay. I will examine the experience and patches for adv7480.

Do you know whether I will see mipi clk sygnal  on the clk wire in case of wrong mipi clock configuration in imx6 processor?

Thanks.

0 项奖励
回复

6,534 次查看
igorpadykov
NXP Employee
NXP Employee

actually adi support suggested easy way to debug that

as described in AN1337 on p.2:

manually program the clock lane of the ADV7280-M, ADV7281-M

to enter and then exit LP mode. The easiest way to do this is by

toggling the CSITX_PWRDN bit (Address 0x00, Bit 7).

Data and clock lanes can enter ulps state independently, for clock lane

one can follow comand given on p.52

http://www.analog.com/media/en/technical-documentation/evaluation-documentation/ADV7280_7281_7282_UG... .

also please check

i.MX6Q video capture issue with ADV7280-M

~igor

0 项奖励
回复

6,534 次查看
kurkinalexandr
Contributor III

I of course tried all of these debug steps.

See below my oscilloscope images.

1) Low state mode: CSITX_PWRDN bit (Address 0x00, Bit 7) contains 1 value.

Mipi data:

IMG_20160502_122426.jpg

Mipi clk:

IMG_20160502_122508.jpg

2) Switching on to high speed mode: set CSITX_PWRDN bit (Address 0x00, Bit 7) in zero value.

Mipi data in high speed mode:

IMG_20160502_122640.jpg

Mipi clk in high speed mode:

IMG_20160502_122734.jpg

Transient process from low power to high speed on mipi clk line:

IMG_20160502_123107.jpg

If I switch on imx6 dphy(mipi_csi2_reset()) after clearing CSITX_PWRDN in ad7280-m, I get 0x200 in State register. If I switch on imx6 dphy before clearing CSITX_PWRDN, I get 0x210 in State register.

3) Just for experience: set both lines to ULPS mode, regarding to ADV7280_7281_7282_UG-637.pdf documet P.52

For both lines:

IMG_20160502_124723.jpg

You can see, that MIPI lines pulled down in real ULPS mode.

I also looked through this brunch i.MX6Q video capture issue with ADV7280-M.

But I think my problem is a little be different, as I can`t see clk sygnal physically. There could be several reasons for this issue:

1) imx6 incorrect terminates mipi clk line. To exclude this version, It could be useful if anybody could show his mipi clk sygnal in case of switched off imx6 dphy and switched on dphy.

2) ad7280 incorrect pass clk sygnal. To exclude this issue I need to get example of clean mipi sygnal  from ADV7280-m with disconnected from mipi slave device wires.

3) hardware issue on my board

Than you for help.

0 项奖励
回复