14.04 is support for which version .bb file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

14.04 is support for which version .bb file

1,197 Views
veeranjaneyulug
Contributor III

HI every one,

Have a great day.

I have one doubt ubuntu version 12.04 support for imx-lib-3.10.17.bb .Like this what about 14.04 for which inx-lib.bb file will support.

Thanks

Labels (6)
0 Kudos
Reply
1 Reply

1,124 Views
igorpadykov
NXP Employee
NXP Employee

Hi veeranjaneyulu

yes ubuntu 12.04 can be used for building 3.10.17 linux, this is described in attached

Freescale Yocto Project User's Guide, Rev L3.10.17_1.0.0-ga  05/2014,

sect.3.1 Host packages.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply