14.04 is support for which version .bb file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

14.04 is support for which version .bb file

1,187件の閲覧回数
veeranjaneyulug
Contributor III

HI every one,

Have a great day.

I have one doubt ubuntu version 12.04 support for imx-lib-3.10.17.bb .Like this what about 14.04 for which inx-lib.bb file will support.

Thanks

ラベル(6)
0 件の賞賛
返信
1 返信

1,114件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi veeranjaneyulu

yes ubuntu 12.04 can be used for building 3.10.17 linux, this is described in attached

Freescale Yocto Project User's Guide, Rev L3.10.17_1.0.0-ga  05/2014,

sect.3.1 Host packages.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信