lvds 24 don't display kernel logo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lvds 24 don't display kernel logo

609 Views
俊宝胡
Contributor I

Hi, i have trouble on the kernel bootup .

i use lvds 24 screen on the sabresd board(YOCTO 3.10.17), on bootup,kernel logo dose't show the screen,it just a black screen.

howerver in linux-3.0.35(ltlib),it show normal.

arch/arm/boot/dts/imx6qdl-sabresd.dtsi

     

        mxcfb1: fb@0 {

                compatible = "fsl,mxc_sdc_fb";

                disp_dev = "ldb";

                interface_pix_fmt = "RGB24";

                mode_str ="LDB-XGA";

                default_bpp = <32>;

                int_clk = <0>;

                late_init = <0>;

                status = "disabled";

        };

driver/video/mxc/ldb.c

     static struct fb_videomode ldb_modedb[] = {

        {

              "LDB-WXGA", 60, 1280, 800, 14065,

              40, 40,

              10, 3,

              80, 10,

              0,

              FB_VMODE_NONINTERLACED,

              FB_MODE_IS_DETAILED,},

        {

              "LDB-XGA", 60, 1920,1080,9734,

              220,25 ,

              21, 10,

              40, 10,

              0,

              FB_VMODE_NONINTERLACED,

              FB_MODE_IS_DETAILED,},

        {

              "LDB-1080P60", 60, 1920, 1080, 7692,

              100, 40,

              30, 3,

              10, 2,

              0,

              FB_VMODE_NONINTERLACED,

              FB_MODE_IS_DETAILED,},

     };

uboot  set

    

       setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,LDB-XGA,if=RGB24,bpp=32 ldb=sin0 video=mxcfb1:off video=mxcfb2:off fbmem=24M

help me ,thanks!

Labels (1)
0 Kudos
1 Reply

391 Views
igorpadykov
NXP Employee
NXP Employee

Hi yiyi

seems udoo LDB WXGA panel has similar characteristics, so one can look at

its integration on:

http://udoo.org/forum/threads/3-10-17-kernel.986/

http://udoo.org/forum/threads/guide-lvds-panel-set-up.843/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos