i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
It is often not easy to use company network to flash application, due to network security (proxy, etc...). We will see in this tutorial, how to flash a Linux application in a SD card with ONLY a SD card reader and simple standard Linux commands. SD card Memory Map A Linux application is divided in 3 parts: the bootloader the Linux Kernel the Linux Rootfs We will flash sequentially these 3 parts Flashing U-boot With the SD card Reader, we will flash the yellow part. In the [...]/ltib/rootfs/boot/ folder $ sudo dd if=u-boot.bin of=/dev/sdb bs=512 skip=2 seek=2 && sudo sync Flashing Linux Kernel With the SD card reader, we will flash the green part. Keep in mind that 1MB=1048576B -> Kernel Offset. $ sudo dd if=uImage of=/dev/sdb bs=1048576 seek=1 && sudo sync Configure U-boot variables To launch the Kernel, you need to configure U-boot. Plug the serial cable on the EVK: 115kbps, 8 bits, 1 stop and no parity EVK switches must be configured as below: DS1 DS2 DS3 DS4 DS5 DS5 DS7 DS8 DS9 DS10 Boot from SD/MMC Card 0 0 0 0 0 0 1 1 0 0 Put the SD card in the EVK (bottom slot) and launch the app. In the hyperterminal type:   BBG U-Boot > printenv To print environnement variables Modify the bootcmd: BBG U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc read 0 ${loadaddr} 0x800 0x1800;bootm' "0x1800" is the size of the kernel. Must be bigger than uImage Kernel file (0x1800x512Byte=3MB) If you want to use the WVGA as display screen (kernel need to be configured with CLAA support), for LTIB1007 and after (before it was 'wvga' option): Script for LTIB1007's u-boot on i.MX51 EVK (copy/paste in the hyperterminal): setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bootm' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw  init=/init' setenv bootargs_base' setenv bootargs console=ttymxc0,115200 di1_primary console=tty1' setenv bootcmd 'run bootcmd_mmc' saveenv Script for LTIB1007's u-boot on i.MX53 EVK (copy/paste in the hyperterminal): setenv bootcmd_mmc 'run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bootm' setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw  init=/init' setenv bootargs_base 'setenv bootargs console=ttymxc0,115200 di0_primary console=tty1' setenv bootcmd 'run bootcmd_mmc' saveenv You must have the following printenv: BBG U-Boot > printenv bootdelay=3 baudrate=115200 loadaddr=0x90800000 netdev=eth0 ethprime=FEC0 uboot_addr=0xa0000000 uboot=u-boot.bin kernel=uImage bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serveri p}:${nfsroot},v3,tcp bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; boot m load_uboot=tftpboot ${loadaddr} ${uboot} ethact=FEC0 bootargs=console=ttymxc0,115200 di1_primary root=/dev/mmcblk0p1 rootwait rw init =/init bootcmd_mmc=run bootargs_base bootargs_mmc; mmc read 0 ${loadaddr} 800 1800 ; bo otm bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw init=/i nit bootargs_base=setenv bootargs console=ttymxc0,115200 di1_primary bootcmd=run bootcmd_mmc stdin=serial stdout=serial stderr=serial</br> Environment size: 748/131068 bytes BBG U-Boot > Create ext3 partition With the SD card reader, create an ext3 partition. You can use gparted, a graphical partition manager tool. Launch gparted: $ sudo gparted Create a new ext3 partition, with 20MB of offset: Copying Linux To copy rootfs folder generated by LTIB, type in the shell: $ sudo cp -r /[…]/ltib/rootfs/* /media/FreescaleSD/ && sudo sync Test application Put the SD in the slot slot and launch the application. Password is root.
查看全文
The Linux L4.1.15_2.1.0 for i.MX 6SLL Release is now available on www.nxp.com.   Files available: # Name Description 1 fsl-yocto-L4.1.15_2.1.0-ga.tar.gz Linux BSP Documentation for L4.1.15_2.1.0. Includes Release Notes, User Guide. 2 L4.1.15_2.1.0-ga_images_MX6SLL.tar.gz i.MX 6SLL EVK Linux Binary Demo Files 3 L4.1.15_2.1.0-ga_mfg-tools.tar.gz i.MX Manufacturing Toolkit for Linux L4.1.15_2.1.0 BSP 4 imx-aacpcodec-4.2.0.tar.gz Linux AAC Plus Codec for L4.1.15_2.1.0   Target boards: i.MX 6SLL EVK Board   Features: See detail features in Release Notes   Known Issues: For known issues and more details please consult the Release Notes.   Information of release, see: README: http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/README?h=imx-4.1-krogoth ChangeLog: http://git.freescale.com/git/cgit.cgi/imx/fsl-arm-yocto-bsp.git/tree/ChangeLog?h=imx-4.1-krogoth
查看全文
Attached is a chunk of the filesystem for the Linux Image https://community.freescale.com/docs/DOC-93887
查看全文
ccache is a C compiler cache. ccache can save a large amount of compilation time on recurring builds and builds restarted from a clean repository after make clean or git clean. It is well suited for e.g. u-boot and Linux compilation. Caching the host compiler Caching "native" builds is easily done by adding in the beginning of your $PATH a special directory, which contains links to ccache to override the usual compiler. On e.g. Debian this directory is readily available as /usr/lib/ccache, So you can do:   $ export PATH="/usr/lib/ccache:$PATH" Typical links found in this folder are:   c++ -> ../../bin/ccache   cc -> ../../bin/ccache   g++ -> ../../bin/ccache   gcc -> ../../bin/ccache etc... Caching the cross compiler Caching cross-compiled builds can be done in the same way as native builds, provided you create links of the form e.g. arm-linux-gnueabihf-gcc pointing to ccache. But there is an even more convenient way for those projects, which rely on a $CROSS_COMPILE environment variable (as is the case for e.g. u-boot and Linux). You can prefix the cross compiler with ccache there in e.g. the following way:   $ export CROSS_COMPILE="ccache arm-linux-gnueabihf-" Monitoring efficiency Now that your builds are cached, you might want to see how much is "spared" with this technique. ccache -s will tell you all sorts of statistics, such as:   cache directory                     /home/vstehle/.ccache   cache hit (direct)                 10852   cache hit (preprocessed)            3225   cache miss                         19000   called for link                    33267   called for preprocessing            9463   compile failed                         3   preprocessor error                     1   couldn't find the compiler           117   unsupported source language          921   unsupported compiler option         2167   no input file                      31681   files in cache                     51694   cache size                           1.3 Gbytes   max cache size                       4.0 Gbytes Here you see a somewhat typical 50%/50% hit/miss ratio. Enjoy! See Also ccache is usually supported natively by build systems, such as Buildroot or Yocto.
查看全文
Introduction to Linux In 1989, a Finnish student called Linus Torvalds started an improvement work of Minix's Kernel, an operational system like Unix wrote by Andrew Tannenbaum, calling his own Kernel as Linux, a mix of Linus and Minix. The main idea about this new Kernel is that it's free. Anyone can develop to improve the Kernel, share the software, change it specific application and distribute without any fee or restriction. All the code is open. Finally, in 1991, Linus launched the first official Linux version, later joining Richard Stallman's GNU project in 1992 with the objective to produce the complete operational system that we know today. Linux had fast success on the x86 architecture and soon it had ported for various processor architectures and became very popular on embedded devices in many different applications like automotive, industrial, telecommunications, consumer and internet appliances. The use of Linux in embedded devices has many advantages: Supports many devices, file systems, networking protocols High portability, since it has been ported for many CPU architectures Large number of ready applications Mature source code with constant actualization Large community of programmers and users over the world testing and adding new features Which Linux distribution should I install on my PC? There are many distributions of Linux available for free. Below are a list of some of them: Ubuntu (IPA: [uːˈbuːntuː] in English,[3][ùbúntú] in Zulu) is an operating system for desktops, laptops, and servers. It has consistently been rated among the most popular of the many Linux distributions. Ubuntu's goals include providing an up-to-date yet stable Linux distribution for the average user and having a strong focus on usability and ease of installation. It is a derivative of Debian, another popular distribution. Ubuntu is sponsored by Canonical Ltd, owned by South African entrepreneur Mark Shuttleworth. The name of the distribution comes from the African concept of ubuntu which may be rendered roughly as "humanity toward others", "we are people because of other people", or "I am who I am because of who we all are", though other meanings have been suggested. This Linux distribution is named as such to bring the spirit of the philosophy to the software world. Ubuntu is free software and can be shared by any number of users. Kubuntu and Xubuntu are official subprojects of the Ubuntu project, aiming to bring the KDE and Xfce desktop environments, respectively, to the Ubuntu core (by default Ubuntu uses GNOME for its desktop environment). Edubuntu is an official subproject designed for school environments, and should be equally suitable for children to use at home. Gobuntu is an official subproject that is aimed at adhering strictly to the Free Software Foundation's Four Freedoms. The newest official subproject is JeOS. Ubuntu JeOS (pronounced "Juice") is a concept for what an operating system should look like in the context of a virtual appliance. Ubuntu releases new versions every six months, and supports those releases for 18 months with daily security fixes and patches to critical bugs. LTS (Long Term Support) releases, which occur every two years, are supported for 3 years for desktops and 5 years for servers. The most recent LTS version, Ubuntu 10.04 LTS (Lucid Lynx), was released on 29 April 2010. The current non-LTS version is 10.10 (Maverick Meerkat) released on 10/10/10 (10 October 2010). Click here for official site Mandriva Linux (formerly Mandrakelinux or Mandrake Linux) is a Linux distribution created by Mandriva (formerly Mandrakesoft). It uses the RPM Package Manager. The product lifetime of Mandriva Linux releases is 18 months for base updates and 12 months for desktop updates. Click here for official site openSUSE, (pronounced /ˌoʊpɛnˈsuːzə/), is a community project, sponsored by Novell and AMD, to develop and maintain a general purpose Linux distribution. After acquiring SUSE Linux in January 2004, Novell decided to release the SUSE Linux Professional product as a 100% open source project, involving the community in the development process. The initial release was a beta version of SUSE Linux 10.0, and as of October 2007 the current stable release is openSUSE 10.3. Beyond the distribution, openSUSE provides a web portal for community involvement. The community assists in developing openSUSE collaboratively with representatives from Novell by contributing code through the open Build Service, writing documentation, designing artwork, fostering discussion on open mailing lists and in Internet Relay Chat channels, and improving the openSUSE site through its wiki interface. Novell markets openSUSE as the best, easiest distribution for all users. Like most distributions it includes both a default graphical user interface (GUI) and a command line interface option; it allows the user (during installation) to select which GUI they are comfortable with (either KDE, GNOME or XFCE), and supports thousands of software packages across the full range of open source development. Click here for official site Fedora is an RPM-based, general purpose Linux distribution, developed by the community-supported Fedora Project and sponsored by Red Hat. Fedora's mission statement is: "Fedora is about the rapid progress of Free and Open Source software." One of Fedora's main objectives is not only to contain free and open source software, but also to be on the leading edge of such technologies. Also, developers in Fedora prefer to make upstream changes instead of applying fixes specifically for Fedora – this ensures that updates are available to all Linux distributions. Click here for official site Debian (pronounced [ˈdɛbiən]) is a computer operating system (OS) composed entirely of software which is both free and open source (FOSS). Its primary form, Debian GNU/Linux, is a popular and influential Linux distribution. It is a multipurpose OS; it can be used as a desktop or server operating system. Debian is known for strict adherence to the Unix and free software philosophies. Debian is also known for its abundance of options — the current release includes over twenty-six thousand software packages for eleven computer architectures. These architectures range from the Intel/AMD 32-bit/64-bit architectures commonly found in personal computers to the ARM architecture commonly found in embedded systems and the IBM eServer zSeries mainframes. Throughout Debian's lifetime, other distributions have taken it as a basis to develop their own, including: Ubuntu, MEPIS, Dreamlinux, Damn Small Linux, Xandros, Knoppix, Linspire, sidux, Kanotix, and LinEx among others. A university's study concluded that Debian's 283 million source code lines would cost 10 billion USA Dollars to develop by proprietary means. Prominent features of Debian are its APT package management system, its strict policies regarding its packages and the quality of its releases. These practices afford easy upgrades between releases and easy automated installation and removal of packages. Debian uses an open development and testing process. It is developed by volunteers from around the world and supported by donations through SPI, a non-profit umbrella organization for various free software projects. The default install provides popular programs such as: OpenOffice, Iceweasel (a rebranding of Firefox), Evolution mail, CD/DVD writing programs, music and video players, image viewers and editors, and PDF viewers. Only the first CD/DVD is necessary for the default install; the remaining discs contain all 26,000+ extra programs and packages currently available. If a user does not wish to download the CDs/DVDs, these extras can be downloaded and installed separately using the package manager. Debian can also be configured to download and install updates automatically. Click here for official site Slackware is a Linux distribution created by Patrick Volkerding of Slackware Linux, Inc. Slackware was one of the earliest distributions, and is the oldest currently being maintained. Slackware aims for design stability and simplicity, and to be the most Unix-like GNU/Linux distribution. Click here for official site
查看全文
NFS Network File System (NFS) is a network file system protocol originally developed by Sun Microsystems in 1984, allowing a user on a client computer to access files over a network as easily as if the network devices were attached to its local disks. The use of NFS makes the development work of user space applications easy and fast since all target root file system is located into host (PC) where the applications can be developed and crosscompiled to target system. The target system will use this file system located on host as if it is located on target. NFS service will be used to transfer the root file system from host to target. NFS resources are listed below: All Boards Deploy NFS All Boards NFS on Fedora NFS on Fedora All Boards NFS on Slackware NFS on Slackware All Boards NFS on Ubuntu NFS on Ubuntu
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342174 
查看全文
Booting Linux Directly from SD/MMC Card     You can create a self-bootable SD or MMC card with Linux.     This tutorial describes how to create a complete Linux system (bootloader + Linux kernel + root file system) that boots from SD/MMC card.     This is very useful for people willing to demonstrate several Linux images that can be self-contained in SD/MMC cards. Flashing RedBoot on MMC using ATK     To boot Linux from a SD card, the first thing to do is to program the bootloader to the card. For this, click on the link below:     I.MX35 PDK Board Flashing SDCard Flashing RedBoot on MMC using DD     You can also use dd on any linux system to load redboot:   $ sudo dd if=./Desktop/mx35_3stack_redboot_mmc.bin of=/dev/sdd bs=512 skip=2 seek=2 Configuring Kernel to Boot From SD/MMC     Creating a Linux bootable MMC/SD Card.     Execute LTIB:   $ ./ltib -c     Choose configure the kernel:   [*] Configure the kernel     Change image generation to NFS:     Target Image Generation     Options --->     (X) NFS only     Compile Linux kernel with built-in support to MMC/SD and ext3:     Follow that sequence:     Device Drivers --->     <*> MMC/SD card support --->     <*> UniFi SDIO glue for Freescale MMC/SDIO     <*> Freescale i.MX Secure Digital Host Controller Interface support       File systems --->     <*> Ext3 journalling file system support     After the compilation copy the file ~/ltib/rootfs/boot/zImage to tftpboot directory:   $ cp ~/ltib/rootfs/boot/zImage /tftpboot Creating RedBoot Kernel Partition     Create RedBoot partitions and copy Linux kernel to it:     Turn MMC active:   RedBoot> factive MMC     Initialize flash partitions:   RedBoot> fis init       RedBoot> fis list     ... Read from 0x07ee0000-0x07eff000 at 0x00060000: .     Name FLASH addr Mem addr Length Entry point     RedBoot 0x00000000 0x00000000 0x00040000 0x00000000     FIS directory 0x00060000 0x00060000 0x0001F000 0x00000000     RedBoot config 0x0007F000 0x0007F000 0x00001000 0x00000000     Load kernel to RAM:   RedBoot> load -r -b 0x100000 /tftpboot/zImage     Using default protocol (TFTP)     Raw file loaded 0x00100000-0x002c31b7, assumed entry at 0x00100000     Create a kernel partition with content of kernel image loaded to RAM:       RedBoot> fis create -f 0x200000 kernel         RedBoot> fis list     ... Read from 0x07ee0000-0x07eff000 at 0x00060000: .     Name FLASH addr Mem addr Length Entry point     RedBoot 0x00000000 0x00000000 0x00040000 0x00000000     FIS directory 0x00060000 0x00060000 0x0001F000 0x00000000     RedBoot config 0x0007F000 0x0007F000 0x00001000 0x00000000     kernel 0x00200000 0x00100000 0x001E0000 0x00100000     If you reset your board you need to see:   Booting from [SD card, CSD Version 1.0]     If instead you see this message:   Booting from [unknown version card ]     This means your card is not support, please replace it with other card. Creating the Root File System     After storing the kernel image in the SD card, remove the card from the target board and insert it in your computer (running Linux).     In this example, Linux detected the SD card as /dev/sdb.     Now we need to create two partitions. The first partition will not be used, this is just reserved to RedBoot and kernel. The second partition will be used to store Linux Root File System.   # fdisk /dev/sdb     Device contains neither a valid DOS partition table, nor Sun, SGI or OSF disklabel     Building a new DOS disklabel with disk identifier 0x526c22da.     Changes will remain in memory only, until you decide to write them.     After that, of course, the previous content won't be recoverable.         Warning: invalid flag 0x0000 of partition table 4 will be corrected by w(rite)         Command (m for help): p         Disk /dev/sdb: 1023 MB, 1023934464 bytes     32 heads, 62 sectors/track, 1008 cylinders     Units = cylinders of 1984 * 512 = 1015808 bytes     Disk identifier: 0x526c22da           Device Boot Start End Blocks Id System     Create the first partition with 8 MB; it already contains RedBoot and the kernel, as we stored previously:             Command (m for help): n     Command action       e extended       p primary partition (1-4)     p     Partition number (1-4): 1     First cylinder (1-1008, default 1):     Using default value 1     Last cylinder, +cylinders or +size{K,M,G} (1-1008, default 1008): +8M     Now, create the second partition using all remaining space on SD card:       Command (m for help): n     Command action       e extended       p primary partition (1-4)     p     Partition number (1-4): 2     First cylinder (10-1008, default 10):     Using default value 10     Last cylinder, +cylinders or +size{K,M,G} (10-1008, default 1008):     Using default value 1008         Command (m for help): p         Disk /dev/sdb: 1023 MB, 1023934464 bytes     32 heads, 62 sectors/track, 1008 cylinders     Units = cylinders of 1984 * 512 = 1015808 bytes     Disk identifier: 0x526c22da     Device Boot Start End Blocks Id System     /dev/sdb1 1 9 8897 83 Linux     /dev/sdb2 10 1008 991008 83 Linux         Command (m for help): w   Now format the second partition as EXT3: # mkfs.ext3 /dev/sdb2   Remove the SD card from your computer and insert again. Probably your Linux distribution will dectect it and will mount automatically.   On Ubuntu 8.10 it was mounted on /dev/media:   # mount   ...   /dev/sdb2 on /media/disk type ext3 (rw,nosuid,nodev,uhelper=hal) If your Linux didn't mount it, then you can mount it manually:   # mkdir -p /media/disk   # mount /dev/sdb2 -t ext3 /media/disk   Enter in your LTIB directory and copy the rootfs content to SD card:   # cd /home/alan/ltib-imx35/rootfs/   # cp -a * /media/disk/   Verify if it was copied correctly:   # ls -l /media/disk/   total 80   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 bin   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 boot   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 dev   drwxr-xr-x 6 root root 4096 2009-03-12 14:41 etc   drwxr-xr-x 3 root root 4096 2009-03-12 09:53 home   drwxr-xr-x 4 root root 4096 2009-03-12 09:55 lib   lrwxrwxrwx 1 root root 11 2009-03-12 14:47 linuxrc -> bin/busybox   drwx------ 2 root root 16384 2009-03-12 14:37 lost+found   drwxr-xr-x 7 root root 4096 2009-03-12 09:53 mnt   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 opt   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 proc   drwxr-xr-x 2 root root 4096 2009-03-12 10:10 root   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 sbin   drwxr-xr-x 2 root root 4096 2009-03-12 09:53 sys   drwxrwxrwt 3 root root 4096 2009-03-12 09:53 tmp   drwxr-xr-x 2 root root 4096 2009-03-12 09:55 unit_tests   drwxr-xr-x 9 root root 4096 2009-03-12 09:55 usr   drwxr-xr-x 11 root root 4096 2009-03-12 09:55 var   root@urubu:~/ltib-imx25/rootfs#     Now umount the SD card:   # umount /media/disk Configuring RedBoot to Load Kernel and Rootfs from SD/MMC Card     Remove the SD card from your computer and place again in the board.     Configure RedBoot to load the kernel from SD/MMC card and set up the kernel command parameter "root" to load the root file system from second SD/MMC card partition (/dev/mmcblk0p2)     RedBoot> fc     Run script at boot: true     Boot script:     Enter script, terminate with empty line     >> fis load kernel     >> exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/mmcblk0p2 init=/linuxrc ip=none"     >>     Boot script timeout (1000ms resolution): 1     Use BOOTP for network configuration: false     Gateway IP address: 10.29.244.254     Local IP address: 10.29.244.135     Local IP address mask: 255.255.0.0     Default server IP address: 10.29.240.182     Board specifics: 0     Console baud rate: 115200     Set eth0 network hardware address [MAC]: false     Set FEC network hardware address [MAC]: false     GDB connection port: 9000     Force console for special debug messages: false     Network debug at boot time: false     Default network device: lan92xx_eth0     Update RedBoot non-volatile configuration - continue (y/n)? y     ... Read from 0x07ee0000-0x07eff000 at 0x00060000: .     ... Erase from 0x00060000-0x00080000: .     ... Program from 0x07ee0000-0x07f00000 at 0x00060000: .       Now just reset the board and it will boot directly from SD/MMC card.
查看全文
Hi all,      I have a problem about usb mass storage driver, that's it can't enumerate my mass storage device.      but it can enumerate my mouse, keyboard...etc hid device.      anyone have idea about it ?      I always get below messages when my mass storage device plugs in.      and below is my dmesg information      My hardware -->      Type A receptacle on otg controller ~
查看全文
GStreamer has a simple feature to enable tracing, allowing the developer to do basic debugging. These can be done in two ways: Adding the parameter --gst-debug=LIST to the pipeline (a pipeline is a executed gst-launch command) Prepending the environment variable GST_DEBUG=LIST' LIST is a a comma-separated argument, indicating the GStreamer elements to trace. For example, if one needs to trace the sink element      $ GST_DEBUG=*sink*:5 gst-launch playbin2 uri=file:///sample.avi or      $ gst-launch playbin2 uri=file:///sample.avi --gst-debug=*sink*:5 Both commands produces the same log. In case want to trace for than one element, so can simple add the <element>:5, for example      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi The number 5 indicates the log category, where 5 is the highest (the most verbose log you can get) and 0 produces no output (5=LOG, 4=DEBUG, 3=INFO, 2=WARN, 1=ERROR). Log can be huge in each pipeline run. One way to filter it is using the grep command. Before grepping, one needs to redirect the standard error to the standard output (GStreamer log goes always to stderr), so      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi 2>&1 | grep <filter string> In case the log needs to be shared, it is important to remove the 'color' of the log, again, one just needs to add the parameter --gst-debug-no-color or prepend the env variable GST_DEBUG_NO_COLOR=1 ----- More shell variables that GStreamer react, can be found here https://developer.gnome.org/gstreamer/0.10/gst-running.html
查看全文
on Host: libx11-dev libpng-dev libjpeg-dev libxext-dev x11proto-xext-dev qt3-dev-tools-embedded libxtst-dev On Target (i.MX device) alsa-utils libpng tslib
查看全文
Getting Started for i.MX53 Quick Start Board Here is a quick overview you can follow to get your very first contact with i.MX53 QSB. Introduction Out of box i.MX53 QSB video booting up Ubuntu Original Video: Out of box i.MX53 QSB video booting up Ubuntu with some demo (GPU and VPU) Original Video: How to load a pre-built image Here, you should have loaded your board with the out-of-box SD card. Next step is create your own SD card with some pre-built image. You can find pre-built image packages from Freescale for Linux look for Linux Binary Demo file Please, go to Timesys wikipage[1] and see how to load a pre-built image. You can use some Freescale image or some Timesys image. Both will work! For loading linux OS you need at least 3 images: bootloader image kernel image root file system image or tarball Bootloader For iMX53QSB the default bootloader provided by Freescale is u-boot.You can build your own image using LTIB following the same procedure from here. Kernel You can build a new uImage (kernel binary image to be loaded by u-boot) using LTIB, and you can follow the instructions from here Root File System Root file system is a set of directories and files that become the system environment. How to Built Your Own Image Take BSP package on Freescale i.MX53 QSB web site. Prepare your computer to LTIB installation, see that you need All Boards LTIB. Transfer all images to the SD Card (it will be placed under <ltib_dir>/rootfs/boot). Configure your u-boot environment variable. Boot your board. In case you want to boot via NFS, please follow the next procedure instead. Take BSP package on Freescale i.MX 53 QSB web site. Prepare your computer to LTIB installation, see that you need @all_boards_ltib Configure your computer to be able to provide NFS service: Configure your TFTP server. Configure your NFS server. Configure your u-boot environment variable. Boot your board. Be aware the kernel command line you set on u-boot variable can configure the display.
查看全文
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343344 
查看全文
gst-inspect is a tool to to get documentation about GStreamer elements. Pipeline Check installed GST elements gst-inspect | tail -1 Check installed FSL GST elements gst-inspect | grep imx Element documentation gst-inspect <gst element>
查看全文
When flashing a Linux System on a SD card using the script mk_mx28_sd on a Ubuntu 12.04 host, one needs to modify it so partitions are created correctly.  Just follow these steps on the console: $ cd $SDK/L2.6.35_10.12.01_SDK_scripts $ cat > first_partition_sector.patch << EOF diff -Naur a/mk_mx28_sd b/mk_mx28_sd --- a/mk_mx28_sd        2010-10-06 09:47:42.000000000 -0500 +++ b/mk_mx28_sd        2012-11-30 13:38:34.508199154 -0600 @@ -178,7 +178,7 @@ n p 1 -1 +2048 +32M t b EOF $ patch -p1 < first_partition_sector.patch then, you can run the mk_mx28_sd command again with the device as parameter                $ cd $LIB $ export PATH=$PATH:$SDK/L2.6.35_10.12.01_SDK_scripts $ mk_mx28_sd /dev/$SDX
查看全文
The solution works when I use mx53_loco bsp. Modify u-boot and kernel, keep the same. Then you may find you can't login into the system regardless of whatever you input after freescale login: It confused me for a long time. If you  also met this problem,try to check the iomux-mx53.h(linux/arch/arm/plat-mxc/include/mach/). #define _MX53_PAD_PATA_DIOW__UART1_TXD_MUX   IOMUX_PAD(the fourth argument 0x878 should be changed to 0x0) I think this is a small bug in header files. Haifeng
查看全文
Change ambient graphic - Ambient Grafic:      Fluxbox (low memory and fast initialization) - Install (root):      apt-get update      apt-get install fluxbox - After instalation, edit file /etc/lightdm/lightdm.conf and change line:      "greeter-session=unity-grreter"  for  "greeter-session=fluxbox"   if, preference auto login comment this line:      "autologin-user=user"  for  "#autologin-user=user" - Reboot and try fluxbox  🙂
查看全文
Attached is a chunk of the filesystem for the Linux Image https://community.freescale.com/docs/DOC-93887
查看全文
The document descript how to use the win32diskimager to create bootable sdcard.  How to resize sdcard mirror rootfs partition. Ex: fsl-image-validation-imx-imx6qpdlsolox.sdcard
查看全文
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
查看全文