i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343017 
View full article
Introduction The Intel® Neural Compute Stick 2 (Intel® NCS 2) is Intel’s newest deep learning inference development kit. Packed in an affordable USB-stick form factor, the Intel® NCS 2 is powered by latest VPU (vision processing unit) – the Intel® Movidius™ Myriad X, which includes an on-chip neural network accelerator called the Neural Compute Engine. With 16 SHAVE cores and a dedicated hardware neural network accelerator, the NCS 2 offers up to 8x performance improvement+ over the previous generation. Ref: https://software.intel.com/en-us/articles/run-intel-openvino-models-on-intel-neural-compute-stick-2   The NCS 2 officially supported hardware platform is x86 PC and Raspberry Pi. In this guide, we will introduce how to implement in i.MX8MQ. Please see attached guide for more details.
View full article
Basic Linear Algebra Subprograms (BLAS) is a specification that prescribes a set of low-level routines for performing common linear algebra operations such as vector addition, scalar multiplication, dot products, linear combinations, and matrix multiplication. OpenBLAS is an optimized BLAS library which is uesd for deep learning accelerator in Caffe/Caffe2. I enable it in Yocto (Rocko) by adding bb file. And I build on i.MX6QP, i.MX7ULP and i.MX8MQ and also run its test example successfully. You can find test example(openblas_utest) under folder image/opt/openblas/bin of OpenBLAS work directory. Currently, version 0.3.0 is supported in the bb file. +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ update to v 0.3.6 and enable mutli-thread by set USE_OPENMP=1 and USE_THREAD=4 when compiling this library.
View full article
Environment:   VMware player 15 + ubuntu 18.04 LTS Reference document: i.MX_Yocto_Project_User's_Guide.pdf 1. Software packages for the compilation # sudo apt-get install flex bison gperf build-essential zlib1g-dev # sudo apt-get install lib32ncurses5-dev x11proto-core-dev # sudo apt-get install libx11-dev lib32z1-dev libgl1-mesa-dev # sudo apt-get install tofrodos python-markdown libxml2-utils xsltproc # sudo apt-get install uuid-dev:i386 liblzo2-dev:i386 gcc-multilib g++-multilib # sudo apt-get install subversion openssh-server openssh-client uuid uuid-dev zlib1g-dev # sudo apt-get install liblz-dev lzop liblzo2-2 liblzo2-dev git-core curl # sudo apt-get install python3 python3-pip python3-pexpect python3-git python3-jinja2 pylint3 # sudo apt-get install u-boot-tools mtd-utils android-tools-fsutils # sudo apt-get install openjdk-8-jdk device-tree-compiler aptitude # sudo apt-get install libcurl4-openssl-dev nss-updatedb # sudo apt-get install chrpath texinfo gawk cpio diffstat # sudo apt-get install libncursesw5-dev libssl-dev libegl1-mesa # sudo apt-get install net-tools python libsdl1.2-dev xterm socat # sudo apt-get install icedtea-netx-common icedtea-netx 2. downloading yocto bsp (L5.4.24_2.1.0) # rm -rf ~/bin # mkdir ~/bin # curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo # chmod a+x ~/bin/repo # export PATH=~/bin:$PATH   # mkdir imx-yocto-bsp-5.4.24-2.1.0 # cd imx-yocto-bsp-5.4.24-2.1.0 # repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.24-2.1.0.xml # cd .repo/manifests # gedit imx-5.4.24-2.1.0.xml          Modify git to https like below:   <remote fetch="https://git.yoctoproject.org/git" name="yocto"/>   <remote fetch="https://github.com/Freescale" name="community"/>   <remote fetch="https://github.com/openembedded" name="oe"/>   <remote fetch="https://github.com/OSSystems" name="OSSystems"/>   <remote fetch="https://github.com/meta-qt5"  name="QT5"/>   <remote fetch="https://github.com/TimesysGit"  name="Timesys"/>   <remote fetch="https://github.com/meta-rust"  name="rust"/>   <remote fetch="https://git.openembedded.org"  name="python2"/>   <remote fetch="https://source.codeaurora.org/external/imx" name="CAF"/> Save it and exit. # cd ~/ imx-yocto-bsp-5.4.24-2.1.0 # repo sync          Begin to compile i.MX8MQ BSP: # DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build-wayland          If users want to use chromium, do it like below, otherwise omit the step.        Add CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" to local.conf        And use 8 thread to compile BSP # gedit ./conf/local.conf …… BB_NUMBER_THREADS =”4” PARALLEL_MAKE =”-j 4” CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" ……          Save it and exit. [comment]          If your ubuntu has 8GB DDR, BB_NUMBER_THREADS can be set to “2”, PARALLEL_MAKE can be set to “-j 2”. # bitbake chromium-ozone-wayland -c fetch # bitbake imx-image-full Use ulimit -n 4096 to solve the issue. Then continue. # bitbake imx-image-full chromium compilation error:          Compile chromium-ozone-wayland separately. # bitbake chromium-ozone-wayland -c cleansstate # bitbake chromium-ozone-wayland -c compile          Use the command to solve the problem. # gedit ../sources/meta-imx/meta-sdk/dynamic-layers/browser-layer/recipes-browser/chromium/chromium-ozone-wayland_%.bbappend DEPENDS += "\         libxkbcommon \         virtual/egl \         wayland \         wayland-native \          mesa         \ "          Add mesa to DEPENDS          Save and exit.          Continue to compile it. # bitbake chromium-ozone-wayland -c compile          done, continue to compile full image   # bitbake imx-image-full Attachment is document in pdf format, which should be clear. NXP TIC team Weidong Sun 08/21/2020
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343059 
View full article
In case you missed our recent webinar, you can check out the slides and comment below with any questions.
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343823 
View full article
NXP i.MX 8 series of application processors support running ArmV8a 64-bit and ArmV7a 32-bit user space programs.  A Hello World program that prints the size of a long int is cross-compiled as 32-bit and as 64-bit from an Ubuntu host and then each is copied to MCIMX8MQ-EVK and run. Resources: Ubuntu 18.04 LTS Host i.MX 8M Evaluation Kit|NXP  MCIMX8MQ-EVK Linux Binary Demo Files - i.MX 8MQuad EVK L4.9.88_2.0.0_GA release Source Code: Create a file with contents below using your favorite editor, example name hello-sizeInt.c. #include <stdio.h> int main (int argc, char **argv) { printf ("Hello World, size of long int: %zd\n", sizeof (long int)); return 0; }‍‍‍‍‍‍‍ Ubuntu host packages: $ sudo apt-get install -y gcc-arm-linux-gnueabihf $ sudo apt-get install -y gcc-aarch64-linux-gnu‍‍‍‍ Line 1 installs the ArmV7a cross-compile tools: arm-linux-gnueabihf-gcc is used to cross compile on Ubuntu host Line 2 install the ArmV8a cross-compile tools: aarch64-linux-gnu-gcc is used to cross compile on Ubuntu host Create Linux User Space Applications Build each application and use the static option to gcc to include run time libraries. Build ArmV7a 32-bit application: $ arm-linux-gnueabihf-gcc -static hello-sizeInt.c -o hello-armv7a‍-static‍‍ Build ArmV8a 64-bit application: $ aarch64-linux-gnu-gcc -static  hello-sizeInt.c -o hello-armv8a‍-static‍‍ Copy Hello applications from Ubuntu host and run on MCIMX8MQ-EVK Using a SDCARD written with images from L4.9.88_2.0.0 Linux release (see resources for image link), power on EVK with Ethernet connected to network and Serial Console port which was connected to a windows 10 PC. Launched a terminal client (TeraTerm) to access console port. Login credentials: root and no password needed. Since Ethernet was connected a DHCP IP address was acquired, 192.168.1.241 on the EVK.  On the Ubuntu host, secure copy the hello applications to EVK: $ scp hello-armv7a-static root@192.168.1.241:~/ hello-armv7a-static                           100%  389KB   4.0MB/s   00:00    $ scp hello-armv8a-static root@192.168.1.241:~/ hello-armv8a-static                           100%  605KB   4.7MB/s   00:00 ‍‍‍‍‍‍‍‍‍‍ Run: root@imx8mqevk:~# ./hello-armv8a-static Hello World, sizeof long int: 8 root@imx8mqevk:~# ./hello-armv7a-static Hello World, sizeof long int: 4‍‍‍‍‍‍‍‍
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342719 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-342877 
View full article
This document is a user guide for the GStreamer version 1.0 based accelerated solution included in all the i.MX 8 family SoCs supported by NXP BSP L5.4.24_1.1.0. Some instructions assume a host machine running a Linux distribution, such as Ubuntu, connected to i.MX 8 device. These commands were tested using Ubuntu 18.04 LTD, and while Ubuntu is not required on the host machine, other distributions have not been tested. These instructions are targeted for use with the following hardware: • i.MX 8MQ EVK • i.MX 8MN EVK • i.MX 8MN EVK • i.MX 8QXP MEK B0 • i.MX 8QM MEK B0   Release History v1.0 - Mar 2020 - Initial release. v2.0 - Sep 2020: Added the following content: - Mux/Demux Examples - Audio Examples - Image Examples - Transcode Examples - Streaming Examples - Multi-Display Examples - Scaling and Rotation Examples - Zero-copy Examples - Debug Examples Maintainers: . Marco Franchi . Pedro Jardim
View full article