This article uses i.MX Linux® User's Guide, Rev. L4.1.15_2.1.0-ga, 05/2017
as an example (it may be found as attachment), please refer to section 4.5.12 (How to build
U-Boot and Kernel in standalone environment).
First, generate a development SDK, which includes the tools, toolchain, and small rootfs to compile against
to put on the host machine.
• Generate an SDK from the Yocto Project build environment with the following command. To set up the Yocto Project build
environment, follow the steps in the i.MX Yocto Project User's Guide (IMXLXYOCTOUG). In the following command,
set <Target-Machine> to the machine you are building for.
<Target-Machine> may be one of the following :
• imx6qpsabreauto
• imx6qpsabresd
• imx6ulevk
• imx6ull14x14evk
• imx6ull9x9evk
• imx6dlsabreauto
• imx6dlsabresd
• imx6qsabreauto
• imx6qsabresd
• imx6slevk
• imx6sllevk
• imx6solosabreauto
• imx6solosabresd
• imx6sxsabresd
• imx6sxsabreauto
• imx7dsabresd
The «populate_sdk» generates an script file that sets up environment without Yocto Project. This SDK should be updated for each release
to pick up the latest headers, toolchain, and tools from the current release.
$ DISTRO=fsl-imx-fb MACHINE=<Target-Machine> source fsl-setup-release.sh -b build-fb
$ DISTRO=fsl-imx-fb MACHINE=<Target-Machine> bitbake core-image-minimal -c populate_sdk
or
$ bitbake meta-toolchain
• From the build directory, the bitbake was run in, copy the sh file in tmp/deploy/sdk to the host machine to build on and execute the
script to install the SDK. The default location is in /opt but can be placed anywhere on the host machine.
Note. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
$ . /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi
or
$ source /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi
From Yocto Project Mega-Manual
Note
By default, this toolchain does not build static binaries. If you want to use the toolchain to build these types of libraries, you need to be sure your image has the appropriate static development libraries. Use the IMAGE_INSTALL variable inside your local.conf file to install the appropriate library packages. Following is an example using glibc static development libraries:
IMAGE_INSTALL_append = " glibc-staticdev"
On the host machine, these are the steps to build U-Boot and Kernel:
• On the host machine, set the environment with the following command before building.
$ export CROSS_COMPILE=/opt/fsl-imx-fb/4.1.15/environment-setup-cortexa9hf-vfp-neon-pokylinux-gnueabi
$ export ARCH=arm
• To build U-Boot, find the configuration for the target boot. In the following example, i.MX 6ULL is the target.
Download source by cloning with
$ git clone http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git -b imx_v2016.03_4.1.15_2.0.0_ga
$ cd uboot-imx
$ make clean
$ make mx6ull_14x14_evk_defconfig
$ make u-boot.imx
• To build the kernel, execute the following commands:
Download source by cloning with
$ git clone http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git -b imx_4.1.15_2.0.0_ga
$ cd linux-imx
$ make defconfig
$ make
• To build an application (Hello World) as test.c:
$ source /opt/fsl-imx-fb/4.1.15-2.0.0/environment-setup-cortexa9hf-neon-poky-linux-gnueabi
$ cd ~/test/
$ arm-poky-linux-gnueabi-gcc --sysroot=/opt/fsl-imx-fb/4.1.15-2.0.0/sysroots/cortexa9hf-neon-poky-linux-gnueabi -mfloat-abi=hard test.c
To check if the the compiled code (a.out) is ARM executable
$ file ./a.out
./a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=0e5c22dcf021748ead2c0bd51a4553cb7d38f6f2, not stripped
Copy file a.out to target Linux filesystem and before run it check again :
root@imx6ul7d:/unit_tests/1# file a.out
a.out: ELF 32-bit LSB executable, ARM, EABI5 version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-armhf.so.3, for GNU/Linux 2.6.32, BuildID[sha1]=0e5c22dcf021748ead2c0bd51a4553cb7d38f6f2, not stripped
To define what Linux libs are needed to run our application :
root@imx6ul7d:/unit_tests/1# ldd a.out
linux-vdso.so.1 (0x7ee93000)
libc.so.6 => /lib/libc.so.6 (0x76e64000)
/lib/ld-linux-armhf.so.3 (0x76f9d000)
If some libs are not located in the filesystem you can observe the following message :
-sh: root@imx6ul7d:/unit_tests/1#./a.out: No such file or directory
Finally - run a.out:
root@imx6ul7d:/unit_tests/1# ./a.out
Hello World
root@imx6ul7d:/unit_tests/1#