Suddenly getting File format not recognized error while compiling Zigbee Control Bridge

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suddenly getting File format not recognized error while compiling Zigbee Control Bridge

1,477 Views
dmsherazi
Contributor IV

Suddenly started getting this error while building the Zigbee Control bridget app Note

dostshah_0-1672664838527.pngdostshah_0-1672664838527.png

c:/nxp/mcuxpressoide_11.6.1_8255/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libm.a: file not recognized: file format not recognized
collect2.exe: error: ld returned 1 exit status
make: *** [Makefile:437: ../../Binaries/ControlBridge_Full_GpProxy_115200/ControlBridge_Full_GpProxy_115200.axf] Error 1
"make TRACE=0 NODE=FULL_FUNC_DEVICE GP_SUPPORT=1 BAUD=115200 -r all" terminated with exit code 2. Build might be incomplete.

 

Although the file does exist and seems to be a valid one

 

dostshah_1-1672665101135.pngdostshah_1-1672665101135.png

 

0 Kudos
Reply
1 Reply

1,457 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @dmsherazi

Hope you are doing well.

Could you please help us with more details?

Which device are you using?

What is your SDK version?

Which version of the Control Bridge Application Note are you using? By any chance, have you modified the source code? Are you able to build the project with no modifications? Have you changed the path of the AN folder?

Regards,
Eduardo.

0 Kudos
Reply