Suddenly getting File format not recognized error while compiling Zigbee Control Bridge

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Suddenly getting File format not recognized error while compiling Zigbee Control Bridge

1,539件の閲覧回数
dmsherazi
Contributor IV

Suddenly started getting this error while building the Zigbee Control bridget app Note

dostshah_0-1672664838527.png

c:/nxp/mcuxpressoide_11.6.1_8255/ide/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m/nofp\libm.a: file not recognized: file format not recognized
collect2.exe: error: ld returned 1 exit status
make: *** [Makefile:437: ../../Binaries/ControlBridge_Full_GpProxy_115200/ControlBridge_Full_GpProxy_115200.axf] Error 1
"make TRACE=0 NODE=FULL_FUNC_DEVICE GP_SUPPORT=1 BAUD=115200 -r all" terminated with exit code 2. Build might be incomplete.

 

Although the file does exist and seems to be a valid one

 

dostshah_1-1672665101135.png

 

0 件の賞賛
返信
1 返信

1,519件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @dmsherazi

Hope you are doing well.

Could you please help us with more details?

Which device are you using?

What is your SDK version?

Which version of the Control Bridge Application Note are you using? By any chance, have you modified the source code? Are you able to build the project with no modifications? Have you changed the path of the AN folder?

Regards,
Eduardo.

0 件の賞賛
返信