Can JN5189HN operate Zigbee and Thread simultaneously?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can JN5189HN operate Zigbee and Thread simultaneously?

ソリューションへジャンプ
2,623件の閲覧回数
andy_kim
Contributor IV

Hello, Community

I'd like to know if JN5189HN can operate Zigbee and Thread simultaneously like WiFi/BT combo module.

If it is available, where can I find the information about it?

 

Thank you.

 

Best regards,

Andy

タグ(1)
0 件の賞賛
返信
1 解決策
2,604件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

I apologize, but  in this case the way to use both stack would be based on the time sharing as there is only one radio in the device, while we do not have examples with Thread and ZigBee working together , you can check the available examples for the K32W for some hybrid examples with BLE and Thread that you can use a a base for the development of the example you are looking for. Still, please take into consideration the memory footprint of both stacks plus the application size.

Regards

元の投稿で解決策を見る

2 返答(返信)
2,580件の閲覧回数
andy_kim
Contributor IV

Dear Estephania,

Thanks for your reply.

 

Best regards,

Andy

 

0 件の賞賛
返信
2,605件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

I apologize, but  in this case the way to use both stack would be based on the time sharing as there is only one radio in the device, while we do not have examples with Thread and ZigBee working together , you can check the available examples for the K32W for some hybrid examples with BLE and Thread that you can use a a base for the development of the example you are looking for. Still, please take into consideration the memory footprint of both stacks plus the application size.

Regards