Vybrid Cortex-M4 Bare Metal L1 Data Cache disable and enable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid Cortex-M4 Bare Metal L1 Data Cache disable and enable

跳至解决方案
4,989 次查看
hjk
Contributor III

When using Vybrid Cortex-M4 bare metal debug, can L1 data cache being disabled? where should I change the setting?

And here're two questions, what's the data cache and instruction cache miss penalty in Systicks ?

Is Systick equals to cycle? Because I measured instruction NOP, it takes 6 systicks

Thanks,

标签 (5)
0 项奖励
回复
1 解答
4,613 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,614 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
4,614 次查看
timesyssupport
Senior Contributor II

Hi,

You can find more about vybrid cortex-M4 cache operation (enable/disable) in "MQX_4_1_1_LINUX_GA/mqx/source/psp/cortex_m/cache.c" with the help of "MQX_User_Guide.pdf" reference manual in MQX_4_1_1_LINUX_GA/doc/mqx.

To enable/access the data cache, need to enable MMC, which is discussed in below thread:

https://community.nxp.com/thread/315672

Thanks,

Timesys Support

4,614 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help to review this case?

0 项奖励
回复