Dual Eth on u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dual Eth on u-boot

跳至解决方案
1,095 次查看
bfac
NXP Employee
NXP Employee

Hello!

Our customer needs to have access to both Vybrid eth ports on u-boot due to safety boot strategy of the system (the system is on 2 different networks at the same time).

Doing tests we have noticed only one eth is supported on u-boot, but when the system boots the kernel, both work fine.

Is there a plan to have the 2 eth controllers functional on u-boot?

Does u-boot support it if configured to do it?

We are using timesys BSP with tower card.

Tks!

Bruno

标签 (3)
0 项奖励
回复
1 解答
915 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Bruno,

As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.

在原帖中查看解决方案

0 项奖励
回复
1 回复
916 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Bruno,

As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.

0 项奖励
回复