Dual Eth on u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Eth on u-boot

Jump to solution
1,820 Views
bfac
NXP Employee
NXP Employee

Hello!

Our customer needs to have access to both Vybrid eth ports on u-boot due to safety boot strategy of the system (the system is on 2 different networks at the same time).

Doing tests we have noticed only one eth is supported on u-boot, but when the system boots the kernel, both work fine.

Is there a plan to have the 2 eth controllers functional on u-boot?

Does u-boot support it if configured to do it?

We are using timesys BSP with tower card.

Tks!

Bruno

Labels (3)
0 Kudos
Reply
1 Solution
1,640 Views
SergioSolis
NXP Employee
NXP Employee

Hello Bruno,

As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.

View solution in original post

0 Kudos
Reply
1 Reply
1,641 Views
SergioSolis
NXP Employee
NXP Employee

Hello Bruno,

As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.

0 Kudos
Reply