Dual Eth on u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,832件の閲覧回数
bfac
NXP Employee
NXP Employee

Hello!

Our customer needs to have access to both Vybrid eth ports on u-boot due to safety boot strategy of the system (the system is on 2 different networks at the same time).

Doing tests we have noticed only one eth is supported on u-boot, but when the system boots the kernel, both work fine.

Is there a plan to have the 2 eth controllers functional on u-boot?

Does u-boot support it if configured to do it?

We are using timesys BSP with tower card.

Tks!

Bruno

ラベル(3)
0 件の賞賛
返信
1 解決策
1,652件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Bruno,

As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,653件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Bruno,

As of today, there are no plans to add Dual Eth on u-boot, though it could be added in the future.

0 件の賞賛
返信