Conflict in IO MUX Configuration for i.MX6 Dual processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Conflict in IO MUX Configuration for i.MX6 Dual processor

1,274 Views
rammanohar
Contributor II

Hello All,

I have problem in configuring the IO Mux pads, when I try to use these particular signals:

SD4_CMD (B17) & SD4_CLK (E16)

NAND_RE_B (B17) & NAND_WE_B (E16)

Since, I have to use both the interfaces uSDHC4 & NAND there is a conflict for these pins.

Can you please suggest any other options available to have both the signals.

Also attached the IOMUX configured file for your review.#

Thanks,

Ram

Labels (1)
0 Kudos
Reply
0 Replies