About EXT_TAMPER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About EXT_TAMPER

跳至解决方案
2,926 次查看
keisukewatanabe
Contributor III

Dear support,

We assume that the EXT_TAMPER0-5 are for access the fuse which is already blown,

can we connect these directly to the GND, in case we don't use this function?

In the reference board, this was connected to the GND via 10Kohm resister,

is this resister necessary?

Best regards,

Keisuke

标签 (1)
1 解答
2,732 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The tamper pins are used as part of the security sub-system for external tamper detection. If they are not being used in your system, you should tie them to ground. The resistors are on the tower board to allow for flexibility of connecting them to VDD to try out the tamper capabilities.

-Anthony

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,733 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The tamper pins are used as part of the security sub-system for external tamper detection. If they are not being used in your system, you should tie them to ground. The resistors are on the tower board to allow for flexibility of connecting them to VDD to try out the tamper capabilities.

-Anthony

0 项奖励
回复
2,732 次查看
naoumgitnik
Senior Contributor V

Dear Keisuke,

Just a small clarification (which originally came from Anthony as well) of why connecting the tamper output pins directly to ground is allowed when they are not used. - By default all the tamper pins are inputs. The active tamper detection has to be enabled for those pins to become outputs.

Sincerely yours, Naoum Gitnik.

0 项奖励
回复
2,732 次查看
keisukewatanabe
Contributor III

Dear Anthony,

Thank you for your reply.

I want to know a detail about the tamper.

Is there a material?

Best regards,

Keisuke Watanabe

0 项奖励
回复
2,732 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Keisuke,

You need Vybrid Security Reference Manual. It can be downloaded from VF6xx Product Summary Page

You need to submit form to request permission to download this item. http://www.freescale.com/webapp/sps/download/mod_download.jsp?colCode=VYBRIDSRM&appType=moderatedWit...

/Jiri

0 项奖励
回复