About EXT_TAMPER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About EXT_TAMPER

Jump to solution
2,884 Views
keisukewatanabe
Contributor III

Dear support,

We assume that the EXT_TAMPER0-5 are for access the fuse which is already blown,

can we connect these directly to the GND, in case we don't use this function?

In the reference board, this was connected to the GND via 10Kohm resister,

is this resister necessary?

Best regards,

Keisuke

Labels (1)
1 Solution
2,690 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The tamper pins are used as part of the security sub-system for external tamper detection. If they are not being used in your system, you should tie them to ground. The resistors are on the tower board to allow for flexibility of connecting them to VDD to try out the tamper capabilities.

-Anthony

View solution in original post

0 Kudos
Reply
4 Replies
2,691 Views
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The tamper pins are used as part of the security sub-system for external tamper detection. If they are not being used in your system, you should tie them to ground. The resistors are on the tower board to allow for flexibility of connecting them to VDD to try out the tamper capabilities.

-Anthony

0 Kudos
Reply
2,690 Views
naoumgitnik
Senior Contributor V

Dear Keisuke,

Just a small clarification (which originally came from Anthony as well) of why connecting the tamper output pins directly to ground is allowed when they are not used. - By default all the tamper pins are inputs. The active tamper detection has to be enabled for those pins to become outputs.

Sincerely yours, Naoum Gitnik.

0 Kudos
Reply
2,690 Views
keisukewatanabe
Contributor III

Dear Anthony,

Thank you for your reply.

I want to know a detail about the tamper.

Is there a material?

Best regards,

Keisuke Watanabe

0 Kudos
Reply
2,690 Views
jiri-b36968
NXP Employee
NXP Employee

Hi Keisuke,

You need Vybrid Security Reference Manual. It can be downloaded from VF6xx Product Summary Page

You need to submit form to request permission to download this item. http://www.freescale.com/webapp/sps/download/mod_download.jsp?colCode=VYBRIDSRM&appType=moderatedWit...

/Jiri

0 Kudos
Reply