About EXT_TAMPER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,949件の閲覧回数
keisukewatanabe
Contributor III

Dear support,

We assume that the EXT_TAMPER0-5 are for access the fuse which is already blown,

can we connect these directly to the GND, in case we don't use this function?

In the reference board, this was connected to the GND via 10Kohm resister,

is this resister necessary?

Best regards,

Keisuke

ラベル(1)
1 解決策
2,755件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The tamper pins are used as part of the security sub-system for external tamper detection. If they are not being used in your system, you should tie them to ground. The resistors are on the tower board to allow for flexibility of connecting them to VDD to try out the tamper capabilities.

-Anthony

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,756件の閲覧回数
anthony_huereca
NXP Employee
NXP Employee

Hi Keisuke,

  The tamper pins are used as part of the security sub-system for external tamper detection. If they are not being used in your system, you should tie them to ground. The resistors are on the tower board to allow for flexibility of connecting them to VDD to try out the tamper capabilities.

-Anthony

0 件の賞賛
返信
2,755件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Keisuke,

Just a small clarification (which originally came from Anthony as well) of why connecting the tamper output pins directly to ground is allowed when they are not used. - By default all the tamper pins are inputs. The active tamper detection has to be enabled for those pins to become outputs.

Sincerely yours, Naoum Gitnik.

0 件の賞賛
返信
2,755件の閲覧回数
keisukewatanabe
Contributor III

Dear Anthony,

Thank you for your reply.

I want to know a detail about the tamper.

Is there a material?

Best regards,

Keisuke Watanabe

0 件の賞賛
返信
2,755件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi Keisuke,

You need Vybrid Security Reference Manual. It can be downloaded from VF6xx Product Summary Page

You need to submit form to request permission to download this item. http://www.freescale.com/webapp/sps/download/mod_download.jsp?colCode=VYBRIDSRM&appType=moderatedWit...

/Jiri

0 件の賞賛
返信