Radar 77Ghz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Radar 77Ghz

Jump to solution
4,407 Views
josephharden
Contributor I

I am a part of a team of students at the University of South Carolina and we are hoping to design a mobile radar application for the university (range of at least 100m). We've looked at 77Ghz modules that are available. Do you have any suggestions on where to start or what we can use?

I'm hoping we can use the modules shown in the video below. (Qorivva MPC577xK MCU and the MRD3000 multi-channel 77 GHz radar transceiver chipset)

77GHz Radar Automotive Safety System - YouTube

We need to obtain the variables that he mentioned in the video and process them using logic. Are there any educational materials available or places to start?

Starting from scratch is a bit daunting. :smileyconfused:

Thanks,

Joseph

Labels (1)
1 Solution
3,700 Views
josephharden
Contributor I

Thank you so much,

I'll be sure to contact her. Thanks again for the help!  :smileyhappy:

View solution in original post

0 Kudos
Reply
2 Replies
3,700 Views
FlavioStiffan
NXP Employee
NXP Employee

dear Joseph

there is no didactic material for the 77GHz radar suite at this point. I would recommend getting in touch with Damaris Ochoa who is managing the Americas relationships with universitieS. She might be able to put you in touch with a professor locally that can help getting you started.

3,701 Views
josephharden
Contributor I

Thank you so much,

I'll be sure to contact her. Thanks again for the help!  :smileyhappy:

0 Kudos
Reply